Back to Event Manager Main Menu

Managing the Pending Events List

Tenant and Site Administrators can use the Pending Events list to manage events that are still in the approval process. You can review, approve, and deny events from this list. Use the Bulk Actions menu to approve multiple events at one time, if needed. You can filter the list of events displayed in the list using the Filters panel on the left side of the screen.

  • Click on Events from the side navigation menu and select Pending Events.

How to Search and Filter the Pending Events List

Use the Search and Filter options to find or show specific events.

Search

  1. Search an event by typing Event Name, Event ID or Keywords in the search bar.

View

  1. Use the View selector to switch between List View, Calendar View, and Timeline View.

  2. The list opens in List View by default unless you have set a different view as your default.

  3. You can use the star icon to set any view as default.

    List View:

    It displays your events as a scrollable list with key details such as event title, ID, dates, and requester. Best for scanning, searching, and taking action on individual events.

    Calendar View:

    It shows events plotted on a calendar, color coded by status. Best for visualizing how events are spread across dates and spotting scheduling gaps or conflicts.

    Timeline View:

    It shows events mapped across a day's hours for each location. Best for seeing how busy a specific facility is briefly and identifying overlapping bookings.

Sort

  1. Use the Sort By drop-down menu to select your preferred primary sorting option for event list.

  2. Sort by drop-down has the following options:

    • A to Z: Sorts events alphabetically by event title (A to Z).

    • Z to A: Sorts events alphabetically by event title (Z to A).

    • Start Date (asc): Sorts events by the earliest start date first.

    • Start Date (desc): Sorts events by the latest start date first.

    • End Date (asc): Sorts events by the earliest end date first.

    • End Date (desc): Sorts events by the latest end date first.

    • Event ID (asc): Sorts events from the lowest to the highest Event ID.

    • Event ID (desc): Sorts events from the highest to the lowest Event ID.

    • Submission Date and Time (asc): Displays events from the oldest to the newest submission.

    • Submission Date and Time (desc): Displays events from the most recent to the oldest submission.

  3. Click away from the data entry box to enable the Apply button.

     

Custom Default Filters

You can define a custom default filter to display when you first navigate to the Pending Events list.

NOTE   These filters are only created for your individual user account and are not shared with other users in Event Manager.

Helpful Tips:

You can add up to 20 custom filters using this method, but only one can be defined as the default filter that will display upon opening the Pending Events list. Additionally, be advised that Event Manager will prioritize the default filter, then stock filters, then any custom user defined filters.

 

 

  1. From the Pending Events list, define the filter criteria you would like to save as part of the default filter.

  2. Click Quick Filter and then select Add Filter.

  3. Enter a Name for this custom filter.

  4. Check the Set as Default box if this should be the default filter that displays when first navigating to this page.

  5. Click Save.

 

Deleting A Custom Filter

  1. Click the pencil icon next to the custom filter you'd like to delete.

  2. Click Delete.

Editing a Custom Filter

  1. Adjust the filters from the Filters side panel.

  2. Click Apply.

  3. Click the pencil icon next to the custom filter you'd like to edit.

  4. Click Save.

How to View Event Details

Events displayed on the pending event list have certain details displayed, such as the Event Title, Event ID, Event Start and End, and Requester. You can also view additional details about an event from the list, such as the Location, Organization, and the Approval Workflow.

  1. Use the Search and Filter options to find or show specific events.
  2. Click anywhere on the event card in the list. A panel will expand that displays more detailed information about the event.

Event Actions

There are a number of actions that can be taken on events in the list, including reviewing, approving, or denying an event.

Helpful Tips:

When managing your events from the Pending Events List, you may see an exclamation mark icon ( or ) next to an event in the list. Be advised, when one of these icons is displayed, it means that action is needed on the event for some reason. Reasons that you may need to take action on an event include:

  • () The event has expired insurance and needs to be updated with current insurance information.
  • ( or ) The event is double booked with another event and one of the two events should be moved. *Note: The red exclamation icon will display only when a location has been set to "Prevent Double Booking".
 

 

  1. Click the Actions drop-down menu on the event you would like to manage.
  2. Select one of the available options under General or Approval:
    • Review Event will open the event form and allow you to review all event details before choosing to Approve, Deny, or Edit the event.
    • Approve will allow you to sign-off on an event, if you are part of the approval process for this event.
    • Force Approve will allow you to bypass the normal approval process and fully approve this event.

      NOTE  This option is only available for Tenant Administrators in Event Manager.

    • Deny will allow you to deny this event and provide a note to the requester to inform them why the event was denied.

How to Bulk Approve Events

You can approve multiple events at the same time using the Bulk Actions menu.

  1. Use the Search and Filter options to find or show specific events.

  2. Check the box next to each event that needs to be approved.

  3. Click on Bulk Actions, and then select Approve from the drop-down menu.

  4. Click one of the buttons at the bottom of the window:

    • Approve All: to sign-off on all selected events.

    • Force Approve: to either approve the events and send them to the next step in the approval process, or approve and publish the events.

    • Cancel: to close the window without making any changes.

Calendar View

To see a month-to-month view of your events, utilize the Calendar View feature. Pending events displayed on the calendar will be color coded as yellow.

 

  • Above the events list, select Calendar View. from the drop-down menu.
  • Events will be displayed on the calendar and color coded according to their status:
    • Approved: Events that have been approved and published will display as green on the calendar.
    • Pending: Events that still require approval will display as yellow on the calendar.
    • Denied: Events that have been rejected will display as red on the calendar.
    • Deleted: Events that have been deleted will display as black on the calendar.
    • Saved: Events that have been saved will display as blue on the calendar.
    • Version: Events that have been versioned during the approval process will display as grey on the calendar.

  • Click on an event from the calendar to open the Event Details panel. You can view relevant event information, review the event or event series, or use the Actions menu to make certain changes to the event.

 

Timeline View

To see the events occurring at your facilities on a particular day, use the Timeline View. You can see where events fall on the timeline for each location to get an at-a-glance idea of how busy a particular location might be.

NOTE   You can only view 100 events at a time, so you may need to filter your event list by Location, Organization, or Category if you have a high concentration of events on a particular day.

  • Above the events list, select Timeline View. from the drop-down menu.

  • The timeline will default to display today's date, but you can change the Start Date under Filters if you'd like to view events for a future date.

  • You can also filter the timeline by other search criteria, such as Location, Organization, Category, or Requester.

  • Events will be displayed on the timeline and color coded according to their status:
    • Approved: Events that have been approved and published will display as green on the timeline.
    • Pending: Events that still require approval will display as yellow on the timeline.
    • Denied: Events that have been rejected will display as red on the timeline.
    • Deleted: Events that have been deleted will display as black on the timeline.
    • Saved: Events that have been saved will display as blue on the timeline.
    • Version: Events that have been versioned during the approval process will display as grey on the timeline.
  • Click on an event from the timeline to open the Event Details panel. You can view relevant event information, review the event or event series, or use the Actions menu to make certain changes to the event.