Back to Event Manager Main Menu

Payment Gateway Configuration

A payment gateway provides a means of processing payments for items sold, such as registrations and products, and allows invoices to be paid online.

Setup registration gateways

Helpful Tips:

Before you begin to set up Payment Gateways for registration payments, you must have your account configured for the gateway you wish to use. This is a separate process from having your account configured for Invoicing. Contact Client Services to start this process.

 

 

Prior to being able to sell items and registrations using Event Manager you will be required to configure your payment gateway. Event Manager supports receiving payments through a number of different vendors, including MySchoolBucks, PayPal, SchoolPay, Stripe, NIC, TrustCommerce, PayFlow Pro, Authorize.Net, and Tempus.

 

  1. Click on Settings from the side navigation menu.
  2. Click on the Payment Gateway Configuration tile under Global Administration.

    NOTE  If you have already set up your Invoice Registration Gateway for MySchoolBucks, PayPal, SchoolPay or Stripe, you do not need to follow the instructions below. Instead, click Setup Invoice Gateway and click Copy to RegistrationInvoice to use the same account for the Registration Invoice Gateway.

 

Setup invoice gateways

Helpful Tips:

Before you begin to set up Payment Gateways for invoice payments, you must have your account configured for the gateway you wish to use. This is a separate process from having your account configured for Registration. Contact Client Services to start this process.

Prior to being able to pay online using Event Manager you will be required to configure your payment gateway. Event Manager supports receiving payments for invoices through a number of different vendors, including MySchoolBucks, PayPal, SchoolPay, Stripe, and Authorize.Net.

  1. Click on Settings from the side navigation menu.
  2. Click on the Payment Gateway Configuration tile under Global Administration.

    NOTE  If you have already set up your Registration Gateway for MySchoolBucks, PayPal, SchoolPay, Stripe, or Authorize.Net, you do not need to follow the instructions below. Instead, Click the Setup Registration Gateway radio button and then click Copy to Invoice to use the same account for the Invoice Gateway.

  3. Select Setup Invoice Gateway from the Invoice Gateway Setup panel.